Development board


The Xsens Avior series Development Board (AVIOR-DEV) exposes the pins of the Avior on the External Connector, a 2.54 mm pitch header, making it easier for the user to test all the features and the peripherals offered by the Avior. Next to that, the AVIOR-DEV has a USB-C connector and two DSUB9 connectors for testing different communication protocols. It also includes 2 mikroBUS™ compatible extension sockets to connect future extensions. This chapter discusses in more detail the connections and peripherals available on the AVIOR-DEV.

 

Overview

The AVIOR-DEV has the following connections as shown in the figure below:

 

Xsens Avior series Development Board overview with connector designators

 

External Connector

The External Connector makes all of the Avior pins available on a 2.54 mm pitch header. These pins can be used to directly interface with an external MCU or transceiver, or to monitor the communication while using the transceivers on the DEV board. Make sure to configure the peripheral and transceiver selection switches properly before driving these signals with an external MCU or transceiver! The pinning of the External Connector can be seen in the following table.

 

Pin descriptions of External Connector

Pin

Avior pin

Name

I/O

Notes

1

1

VIN

PWR

Supplies VDDA with 3.3 V 

2

2, 4, 12 

GND

PWR

 

3

3

VDDIO_IN

PWR

Supplies VDDIO 

4

2, 4, 12

GND

PWR

 

5

5

RSV

O

Reserved for future use 

6

7

RSV

I

Reserved for future use 

7

9

SEC_TX/CAN_TX

O

NC if SEL = 1x and SW2 = UP (int. CAN) 

8

11

SEC_RX/CAN_RX 

I

NC if SEL = 1x and SW2 = UP (int. CAN) 

9

2, 4, 12

GND

PWR

 

10

2, 4, 12

GND

PWR

 

11

13

MAIN_TX/SCK/ADDR0

I/O

Multi-protocol pin depending on peripheral selection 

12

14

MAIN_RX/nCS/ADDR1 

I

Multi-protocol pin depending on peripheral selection 

13

15

MAIN_RTS/DE/MISO/ADDR2 

I/O

Multi-protocol pin depending on peripheral selection 

14

16

MAIN_CTS/MOSI/ADDR3

I

Multi-protocol pin depending on peripheral selection 

15

2, 4, 12

GND

PWR

 

16

2, 4, 12

GND

PWR

 

17

8

SCL

I

Do not use as peripheral selection pin! 

18

10

SDA

I/O

Do not use as peripheral selection pin! 

19

6

DRDY

O

Data ready output for SPI and I2C communication 

20

-

FTDI_CBUS0 

I/O

Connected to CBUS pin of FTDI chip (USB) 

21

17

SYNC_IN1 

I

Synchronization input 1

22

18

SYNC_IN2 

I

Synchronization input 2

23

20

SYNC_OUT 

O

Synchronization output 

24

-

GNSS PPS 

O

GNSS PPS output 

 

Power

The Avior-DEV can be supplied by USB or through the External Connector. The VDDA of the Avior will always be supplied with a 3.3 V voltage. The VDDIO to the Avior will default to 1.8 V in case it is not supplied by VDDIO_IN. In case the VDDIO_IN on the External Connector is used, the VDDIO voltage on the Avior will have the voltage supplied on that pin (overruling the VDDIO from the USB power). 

 

Host connections

Note that the selection switches need to be set before powering the Avior-DEV.
When using the transceivers on the Avior-DEV for USB, RS232, RS422 or CAN, the communication pins on the External Connector should not be driven.

 

UART

The main UART, including flow control, can be connected to pins 11 to 14 on the External Connector as shown in the table above. When flow control is not used, the CTS pin (pin 14 on the External Connector) can be connected to ground or the peripheral selection switch can be set to 01. The following table shows the required switch configuration to use the direct UART communication.

 

Switch configuration for enabling UART

Switch

Flow control

No flow control

SEL

00 (default)

01

SW1

Up (Ext. UART) 

Up (Ext. UART) 

SW2

-

-

 

SPI

The same pins on the External Connector that are used for the main UART can also be used for SPI when the peripheral selection is set accordingly. The following table shows the required switch configuration to use the SPI communication.

 

Switch configuration for enabling SPI

Switch

SPI (CAN)

SEL

10

SW1

Up (Ext. UART)

SW2

-

 

When using SPI, the DRDY pin on the External Connector (pin 19) can be used as a data ready pin, indicating new messages are available to be read by the host.

 

I2C

The I2C pins on the External Connector can be used for I2C communication when the peripheral selection is set accordingly. The following table shows the required switch configuration to use the I2C communication.

 

Switch configuration for enabling I2C

Switch

SPI (CAN)

SEL

11

SW1

Up (Ext. UART)

SW2

-

 

When using I2C, the DRDY pin on the External Connector (pin 19) can be used as a data ready pin, indicating new messages are available to be read by the host, and the first three ADDR pins (pins 11 to 13) can be used to set the I2C address (pin 14 is reserved). The table below shows the different supported I2C addresses (7 bit, without the read/write bit).

 

Supported addresses for I2C

I2C address

A2

A1

A0

0x1D

0

0

0

0x1E

0

0

1

0x28

0

1

0

0x29

0

1

1

0x68

1

0

0

0x69

1

0

1

0x6A

1

1

0

0x6B (default)

1

1

1

 

USB

The USB-C port on the Avior-DEV can be used to connect the Avior to a host through the included USB-A to USB-C cable. The USB device requires the drivers that are automatically included when downloading the MT Software Suite. The following table shows the required switch configuration for this connection.

 

Switch configuration USB

Switch

Position

SEL

00 (default)

SW1

Down (default)

SW2

-

 

RS232/422

The upper DSUB9 female connector (next to the USB-C) can be used to connect to either a RS232 or RS422 peripheral. The following figure and table show the pinning of this DSUB9 connector. Note that the pinning is the same as on the 600-series development board for the RS232 signals, but different for the RS422 signals. Pin 9 is by default not connected, but can be connected to VIN by placing a zero-Ohm resistor on R3.

 

Make sure not to supply VIN by both the External Connector and this DSUB9 connector at the same time!

 

Pinout of DSUB9 connector RS232/422

 

DSUB9 connector 2 pinning for RS232/422

Pin

RS232

RS422

I/O

Description

2

TXD

TXD-

O

Transmit output (negative RS422 output)

3

RXD

RXD+

I

Receiver input (positive RS422 input)

5

GND

GND

PWR

 

7

CTS

RXD-

I

Clear to send input (negative RS422 input)

8

RTS

TXD+

O

Ready to send output (positive RS422 output)

9

(VIN)

(VIN)

(PWR)

Optional (when R3 is placed)

 

 

The following table shows the required switch configuration for the RS232 and RS422 connections.

 

Switch configuration for enabling RS232/422

Switch

RS232

RS422

SEL

00 (default)

01

SW1

Middle (RSxxx)

Middle (RSxxx)

SW2

-

-

CAN

The lower DSUB9 female connector can be used to connect a CAN bus to the Avior. The table below shows the pinning of this connector. The CAN bus interface includes a 120 Ohm termination resistor on the Avior-DEV (R4), which can be removed if required. The following figure and table show the pinning of this DSUB9 connector. Pin 9 is by default not connected but can be connected to VIN by placing a zero-Ohm resistor on R5.

 

Make sure not to supply VIN by both the External Connector and this DSUB9 connector at the same time!

 

Pinout of DSUB9 connector CAN

 

DSUB9 connector 1 pinning for CAN

Pin

Name

I/O

Description

2

CANL

I/O

CAN low

5

GND

PWR

 

7

CANH

I/O

CAN high

9

(VIN)

(PWR)

Optional (when R5 is placed)

 

The following table shows the required switch configuration for the CAN connection on the DSUB9 connector.

 

Switch configuration for enabling CAN (with internal transceiver)

Switch

CAN

SEL

1x

SW1

-

SW2

Up (Int. CAN)

 

 

When you want to connect your own CAN transceiver instead of using the transceiver on the Avior-DEV, you need to configure the switches as shown in the table below. 

Switch configuration for enabling CAN (without internal transceiver)

Switch

External CAN

SEL

1x

SW1

-

SW2

Down (Ext. CAN)

 

External GNSS extension socket and daughter card (Avior (RTK) GNSS-INS DK only)

The  (primary) GNSS extension socket has mikroBUS™ compatible pinning. This enables the user to connect alternate GNSS daughter card modules with mikroBUS™ pinning to the Avior DEV. The pinning connections for the GNSS extension socket are listed in the table below. The extension uses the 5V supply pin by default, which is connected to the 5V that is generated on the Avior DEV (the IO voltages are on 3.3 V). 

 

Connections on (primary) GNSS extension socket

Pin 

Mikro BUS 

Avior 

Pin 

Mikro BUS 

Avior 

P200-1 

AN 

NC 

P201-1 

PWM 

NC 

P200-2 

RST 

Pull-up 

P201-2 

INT 

SYNC_IN2 

P200-3 

CS 

NC 

P201-3 

TX 

GNSS_RxD 

P200-4 

SCK 

NC 

P201-4 

RX 

GNSS_TxD 

P200-5 

MISO 

NC 

P201-5 

SCL 

RFU 

P200-6 

MOSI 

NC 

P201-6 

SDA 

RFU 

P200-7 

3.3V 

NC 

P201-7 

5V 

5V 

P200-8 

GND 

GND 

P201-8 

GND 

GND 

 

 

XBee socket pinning 

Pin 

GNSS board 

P202-1 

VRADIO (3V3, max. 300 mA) 

P202-2 

RTCM_RxD 

P202-3 

RTCM_TxD 

P202-[4..9] 

NC 

P202-10 

GND 

P203-[11..20] 

NC 

 

 

GNSS RTK

 

 

Electrical specifications

 

AVIOR-DEV power supply specifications

Power

Min

Typ

Max

Unit

Remarks

VUSB

4.5

5

5.5

V

USB connector

VVIN

3.2[1]

 

5.1

V

External Connector and DSUB 

VVDDIO_IN

1.7

 

3.4

V

External Connector 

IIN @ 5V

 

100

500

mA

USB, External Connector and DSUB 

IOUT, SOCK

 

 

250

mA 

Maximum total current output through the extension sockets

IOUT,DSUB

 

 

500

mA

Maximum total current output through DSUB connector power pins when R3 and/or R5 are placed


[1] The VIN must be 4.5 V minimum when extension boards are connected without USB supply!

 

AVIOR-DEV interfaces electrical specifications

Interface

Symbol

Min

Typ

Max

Unit

Description

CAN

VI(DIFF)(R) 

-4.0

 

0.5

V

Recessive differential input voltage 

-12V < V(CANH, CANL) < +12V 

 

VI(DIFF)(D) 

0.9

 

9.0

V

Dominant differential input voltage 

-12V < V(CANH, CANL) < +12V 

 

VO(DIFF)(R) 

-500

0

50

mV

Recessive differential output voltage 

VI(DIFF)(D) 

-1.3

2.0

5.0

V

Dominant differential output voltage  

VO(L)(D) 

0.5

1.5

2.25

V

CANL dominant output voltage  

VO(H)(D)

2.75

3.5

4.5

V

CANH dominant output voltage 

RTERM 

110

120

140

Ω

Termination resistance (when enabled) 

RS232

VIL 

-15

 

0.6

V

Low input voltage 

VIH

2.0

 

±15

V

High input voltage  

VIN

3

5

7

kΩ

Input resistance 

VOT

±5.0

±5.5

 

V

Driver output voltage swing  

RS422

VCM_IN

-7

 

12

V

Input common mode voltage 

VTH

-200

-125

-50

mV

Differential input voltage threshold 

ΔVTH 

 

25

 

mV

Input hysteresis voltage 

RIN

96

 

 

kΩ

Input resistance (with termination disabled) 

RTERM

100

120

150

Ω

Termination resistance (when enabled)  

VOD

1.5

 

3.3

V

Differential output voltage (RL = 54 Ω) 

VCM_OUT

 

 

3 

V

Output common mode voltage

EXT_IN[2]

VIL 

0

 

0.15

V

Low input voltage on External Connector 

VIH

VDDIO-0.2 

 

3.6 

V

High input voltage on External Connector 

EXT_OUT[2]

VOL 

0

 

0.4

V

Low output voltage on External Connector (1 mA sink)  

VOH

0.8*VDDIO 

 

VDDIO

V

High output voltage on External Connector (-20 μA source) 


[2] When using only USB for power, VDDIO is 1.8 V. 

 

Absolute maximum ratings

 

Absolute maximum ratings AVIOR-DEV

Parameter

Symbol

Min

Max

Unit

Comments

Power input voltage 

VIN

-0.3

6

V

For all power inputs (USB, External Connector and DSUB)

CAN DC 

VCAN_DC

-58

58

V

Common mode voltage of CAN_H and CAN_L with respect to ground

CAN Differential 

VCAN_DIFF

-17

17

V

Differential voltage between CAN_H and CAN_L

RS232/RS422 inputs 

VRS232

-18

18

V

 

EXT inputs 

VI

-0.3

5.5

V

Input voltage on External Connector pins

EXT outputs 

IO

 

±40

mA

Output current on External Connector pins

ESD protection 

 

 

±2000

V

Human body model

 

 

Stresses beyond those listed under “Absolute Maximum Ratings” may cause permanent damage to the device. These are stress ratings only. Functional operation of the device in these or any other conditions beyond those indicated in the operational sections of the specifications is not implied. Exposure to absolute maximum rating conditions for extended periods may affect device reliability and lifetime.

 

Development Board Drawing

The following figures show the dimensions of the Avior-DEV. All dimensions are in mm. 

 

Avior-DEV Development Board drawing (Top and Side view)

 

Create your own Knowledge Base