This document provides hardware design instructions for the Xsens Avior OEM trackers (A#X##C). The Xsens Avior OEM trackers are plastic (IP51) devices which can be connected to a host through SPI, I2C, UART, or CAN(-FD) interface, or through USB using the USB connection cable (included in the Avior series Development Kit).
The Xsens Avior series Datasheet provides information on the usage and technical details of the Avior series.
The Family Reference Manual supplements this document. It reports generic information on the Xsens generic products, such as output definitions, algorithm details and installation tips.
For testing and prototyping, Xsens provides the Avior series Development Kits (DK). In addition to the SPI, I2C, UART, CAN(-FD), the Development Kit comes with a USB connection cable. Technical details of the Development Kit and its usage can be found in the Xsens Avior series Development Kit User Manual.
The MT Low Level Communication Protocol Document provides a complete reference for the protocols used to communicate with Xsens Motion Trackers on a low-level basis. The MT Low Level Communication Protocol Document also describes the synchronization messages and settings in detail.