The development kit is a very easy to use starter’s kit that allows for fast and easy integration of the sensor in any user scenario. The figure below shows a typical Development Kit, containing an Xsens motion tracker. All software and installation instructions are available online via http://www.xsens.com/setup.
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvaW1hZ2UoNSkucG5nIiwiQ29uZGl0aW9uIjp7IkRhdGVMZXNzVGhhbiI6eyJBV1M6RXBvY2hUaW1lIjoxNzg2MTExMDA4fX19XX0_&Signature=ePnzxcUvEuKYRZLSi18UUuvKsKpa-bYdKrJXb9GrHoABleT5fF~kpoNa6UAWpmvsqMDj0IEL1c7f7MbTunlf8uU09GG8PlmQEJiS~lXNUpkNFZHiX9Vb3tmso3BTMTX1miQ9iw5zRZa-BbjXz5XMDuMjI1YrL1ytDIGCEPnlEfbayIJAbwBmQphVy9s6c9Al4nbkAqaV3tz9jieoiav4v2ykjmMbERj7lqgx2k-hoqCmjJeKIxPKHP3jHn9Phh7UUCyG23~tFqDofPbHhlHN7fKRJbV7TwQwZVGDOyA4jEeCDumq~meLfis3A~yUGwX8Not7tVAerV5~dxrWlw3B5A__&Key-Pair-Id=K2TK3EG287XSFC)
Development Kit
Depending on the model you have purchased, the Development Kit can contain any of the following items:
|
Component |
Description |
|---|---|
|
A Motion Tracker |
|
|
Development board |
A tool for prototyping and validation |
|
(micro) USB (converter) cable or dongle |
A cable or dongle to connect the device to a USB port |
|
multi-purpose (flat) cable |
A cable which exposes all physical lines to a device |
|
GNSS daughter card |
An accessory which fits the MTi 1-series and MTi 600-series development board which contains a GNSS receiver (click-boardTM compatible) |
|
GNSS antenna |
|
|
Test and Calibration certificate |
|
|
Component |
Description |
|---|---|
|
MT Software Suite (MTSS) |
available for download via http://www.xsens.com/setup |
|
Xsens USB driver
|
Part of the MTSS |
|
MT Manager for Linux and Windows |
Part of the MTSS |
|
MT Software Development Kit (MT SDK) for multiple OS |
Part of the MTSS, containing the following components:
|
|
Magnetic Field Mapper – MFM (Windows and Linux) |
Part of the MTSS, containing the following component:
|
|
Firmware Updater |
Separate component design to update the device firmware |
|
Documentation |
Part of the MTSS, PDFs are available online, containing the following components:
|
|
MFM SDK Library |
Library for the Magnetic Field Mapper |
|
NOTE: the most recent version of the software, firmware updater, source code and documentation can always be downloaded on www.xsens.com/software-downloads.
|
The easiest way to get started with your device is to use MT Manager. MT Manager is a software tool to easily get to know and to demonstrate the capabilities of the sensor and to configure the device to suit your needs.
Additionally, MT Manager allows you to:
Please refer to the MT Manager User Manual for more information on MT Manager.
The Xsens Device API (XDA) serves as a starting point for system integrators interested in assessing the basics of the SDK. The main objective of the SDK is to facilitate the development of user-specific host applications based on Xsens motion trackers.
The MT Software Development Kit (MT SDK), part of the MT Software Suite installation, provides examples based on XDA for multiple programming languages. These programming examples can be used as a starting point for further software development.
The MT SDK (and the MT Software Suite) is designed for the MTi 1-series, MTi 10-series, MTi 100-series, MTi 600-series, Xsens Avior series and Xsens Sirius series. See also: Introduction to the MT SDK programming examples for MTi devices
The low-level communication protocol (named Xbus protocol) offers full control and functionality. It is essential on platforms that do not support the Xsens Device API, such as custom embedded computers and microcontrollers.
The low-level communication is extensively described in the MT Low-Level Communication Protocol Documentation. Next to that, source code is delivered to make driver development and Xbus message parsing for the motion tracker as easy and quick as possible.
New firmware versions for products are released several times per year. A release notification will be included in the Xsens newsletter, including all changes made with respect to the previous firmware version. A complete history of firmware releases is available on our Knowledge Base: MTi Release Notes and Changelogs
Public firmware versions can be divided into two categories:
|
Component |
Disclaimer |
|---|---|
|
Beta firmware |
Caution! This in-development version of software and/or firmware may be unstable and contain bugs. Your valuable feedback will help us to create the best software possible. Before you start using the software and/or firmware, please be aware that:
|
The firmware of the industrial motion trackers can be updated (or downgraded to an older version) using the Firmware Updater, which can be downloaded from the Xsens website: https://www.xsens.com/software-downloads.
An embedded firmware updater is available specifically for MTi 1-series devices that have been designed-in without the possibility to connect with a PC. It can be found in the MT SDK folder of your MT Software Suite.
The installer of the MT Software Suite can install 4 components: MT Manager, MT SDK, Magnetic Field Mapper (MFM) and MFM SDK. The Firmware Updater is a separate installer. The MT Software Suite has a Restricted License Agreement that you need to accept. In the table below, the conditions for use of each component are summarized.
|
Component |
Conditions |
|---|---|
|
MT Manager |
For use with Xsens products only Not allowed to re-distribute Not allowed to reverse engineer Not allowed to modify |
|
MT SDK |
For use with Xsens products only Allowed to re-distribute “as is” or embed in programs Not allowed to reverse engineer Allowed to execute, reproduce, modify and compile (modified) source code to use with Xsens products only Not allowed to modify DLL Include License Agreement with distribution |
|
MFM |
For use with Xsens products only Allowed to re-distribute “as is” Not allowed to reverse engineer Not allowed to modify Include License Agreement with distribution |
|
MFM SDK |
For use with Xsens products only Allowed to re-distribute “as is” or embed in programs Not allowed to reverse engineer Allowed to execute, reproduce, modify and compile (modified) source code to use with Xsens products only Not allowed to modify DLL Include License Agreement with distribution |
|
FWU |
For use with Xsens products only Allowed to re-distribute “as is” Not allowed to reverse engineer Not allowed to modify Include License Agreement with distribution |