System Overview


Test and Calibration

A correct calibration of the sensor components inside the industrial motion tracker is essential for an accurate output. The quality and importance of the calibration are of highest priority. Each Xsens’ industrial motion tracker is calibrated and tested by subjecting each device to a wide range of motions and temperatures.

 

The individual calibration parameters are used to convert the sensor component readout (digitized voltages) to physical quantities as accurately as possible, compensating for a wide range of deterministic errors. Additionally, the calibration values are used in Xsens sensor fusion algorithms, as discussed later in this document.

 

Each industrial motion tracker contains individual test and calibration data in its eMTS (extended Motion Tracker Settings). It is digitally signed by a Test Person and states the calibration values determined during the calibration of the industrial motion tracker at Xsens’ calibration facilities. The values can be seen by connecting the industrial motion tracker to MT Manager and navigating to Device Settings → Modelling Parameters.

 

Next to the calibration values shown in MT Manager, each device is calibrated according to more complicated models to ensure accuracy (e.g. non-linear temperature effect, cross coupling between acceleration and angular rate[1]).

 

 

Physical sensor model

This section explains the basics of the individual calibration parameters of each industrial motion tracker .

 

The physical sensors inside the industrial motion tracker (accelerometers, gyroscopes and magnetometers)[6] are all calibrated according to a physical model of the response of the sensors to various physical quantities, e.g. temperature. The basic model is linear and according to the following relationship:

 

(s=K_T^{-1}(u-b_T))

 

During factory calibration, a unique gain matrix, KT and the bias vector, bT, are assigned to each industrial motion tracker. This calibration data is used to relate the sampled digital voltages, u, from the sensors to the respective physical quantity, s.

 

The gain matrix is split into a misalignment matrix, A, and a gain matrix, G. The misalignment specifies the directions of the sensitive axes with respect to the ribs of the sensor-fixed coordinate system (Sxyz) housing. E.g. the first accelerometer misalignment matrix element a1,x describes the sensitive direction of the accelerometer on channel one. The three sensitive directions are used to form the misalignment matrix:

 

 

With O representing higher order models, temperature modelling, g-sensitivity corrections, etc.

 

Each individual industrial motion tracker is modeled for temperature dependence of both gain and bias for all sensors and other effects. This modeling is not represented by the simple model in the above equations but is implemented in the firmware with the temperature coefficient being determined individually for each device during the calibration process. The basic indicative parameters in the above model of your individual industrial motion tracker can be found in MT Manager (Device Settings dialog).

 

 

Coordinate systems

Data from the industrial motion tracker is represented in various coordinate systems, which are explained below.

 

Calibrated inertial data and magnetic field data

The default sensor-fixed frame (Sxyz) is a right-handed Cartesian coordinate system that is fixed to the device. When the sensor is rigidly attached to another object or vehicle but not aligned, it may be convenient to rotate the sensor coordinate system Sxyz to an object coordinate system (Oxyz).

Refer to BASE: MTi reference co-ordinate systems for more information on the available orientation resets.

 

Sxyz or Oxyz are the coordinate frames used to express the rate of turn, acceleration and magnetic field outputs. The encased version of the industrial motion tracker shows Sxyz on the sticker. Figure Default coordinate system of MTi 1-series and Figure Default coordinate system of MTi 600-series, Xsens Avior series and Xsens Sirius series depict the sensor coordinate system on the MTi 1series, MTi 600-series, Xsens Avior series and Xsens Sirius series . Later in this document, small x, y and z are the axes labels for Sxyz and Oxyz. Capital X, Y and Z stand for the local-earth fixed coordinate system (LXYZ).

 

Default coordinate system of MTi 1-series

xXz+SgAAAABJRU5ErkJggg==

A close-up of a boxAI-generated content may be incorrect., Picture

Default coordinate system of MTi 600-series, Xsens Avior series and Xsens Sirius series

 


The housing and PCB of the MTi 600-series, Xsens Avior series and Xsens Sirius series are carefully aligned with the output coordinate system during the individual factory calibration. The non-orthogonality between the axes of Sxyz is <0.05°. This also means that the output of 3D linear acceleration, 3D rate of turn and 3D magnetic field data all will have orthogonal xyz readings within <0.05°.

 

Some of the commonly used data outputs and their reference coordinate systems are listed in the table below.

 

Data outputs with reference coordinate systems

Data

Reference coordinate system

Details

Acceleration

Sensor-fixed frame (Sxyz) or Oxyz

Calibrated inertial data and magnetic field data

Rate of turn

Sensor-fixed frame (Sxyz) or Oxyz

Calibrated inertial data and magnetic field data

Magnetic field

Sensor-fixed frame (Sxyz) or Oxyz

Calibrated inertial data and magnetic field data

Velocity increment

Sensor-fixed frame (Sxyz) or Oxyz

Orientation increment and Velocity increment (dq and dv)

Orientation increment

Sensor-fixed frame (Sxyz) or Oxyz

Orientation increment and Velocity increment (dq and dv)

Free acceleration

Local earth-fixed frame (LXYZ), default ENU

Free acceleration

Orientation

Defined as the difference between Sensor-fixed frame ((Sxyz) or Oxyz) and local earth-fixed frame (LXYZ), default ENU

Orientation data

Velocity

Local earth-fixed frame (LXYZ), default ENU

Velocity data

Position

Local earth-fixed frame (LXYZ), default ENU

Position data

 

 

 

Orientation data

By default, the local earth-fixed reference coordinate system LXYZ is defined as a right-handed Cartesian coordinate system with[2]:

 

 

This coordinate system is known as ENU (East-North-Up) and is the standard in inertial navigation for aviation and geodetic applications. See the figure below for a visualization. Note that it is possible to change LXYZ into a different convention, like NWU (North-West-Up) or NED (North-East-Down), by changing an alignment matrix or applying an orientation reset. Refer to BASE: MTi reference co-ordinate systems for more information on the available orientation resets.

 

 

Visualization of the local earth-fixed coordinate system (LXYZ) and Position representation systems WGS84 (φ, λ) and ECEF (Xecef, Yecef, Zecef)

 

The 3D orientation output is defined as the orientation between the body-fixed coordinate system, Sxyz or Oxyz, and the local earth-fixed co-ordinate system, LXYZ.

 

Orientation output modes

The output orientation can be presented in different equivalent representations:

 

 

A positive rotation is always “right-handed”, i.e. defined according to the right-hand rule (corkscrew rule), see Figure Right hand rule. This means a positive rotation is defined as clockwise in the direction of the axis of rotation.

 

https://upload.wikimedia.org/wikipedia/commons/4/45/Right_hand_rule_simple.png

Right hand rule

 

Refer to BASE by Xsens to find more information on how quaternions, Euler angles and the rotation matrix relate to each other.

 

 

Interpretation of yaw as heading

With the default ENU LXYZ coordinate system, the industrial motion tracker's yaw output is defined as the angle between East (X) and the horizontal projection of the sensor roll axis (x), positive about the local vertical axis (Z) following the right-hand rule [4]. The table below shows the different yaw values corresponding to the different local coordinate systems that are available for the industrial motion tracker.

 

Yaw in different coordinate systems (applies only to AHRS and GNSS/INS product types). The industrial motion tracker is assumed to be mounted with its roll-axis (X) aligned with the roll-axis of the vehicle (front of the vehicle).

Local coordinate system (output)

Roll-axis of the vehicle

Yaw value

East-North-Up (ENU, default)

Pointing North

90 deg

East-North-Up (ENU, default)

Pointing East

0 deg

North-West-Up (NWU)

Pointing North

0 deg

North-East-Down (NED)

Pointing North

0 deg

 

When using the ENU convention (default), the yaw output is 0º when the vehicle (x-axis of the industrial motion tracker) is pointing East (X axis of LXYZ). When it is required that the yaw output is 0º when the x-axis of the industrial motion tracker is pointing north, it is recommended to select NWU or NED as the local coordinate system. In article Changing or resetting the MTi reference co-ordinate systems the various alignment resets are described.

 

When using the GNSS/INS products in an automotive application, as best practice, pay proper attention to mounting of the industrial motion tracker on the automotive platform/vehicle. It is recommended to always mount the device with the x-axis pointing to the front of the vehicle irrespective of the local coordinate frame used for the output data.

 

True North vs. Magnetic North

As defined above, the output coordinate system of the industrial motion tracker is with respect to local Magnetic North. The deviation between Magnetic North and True North (known as the magnetic declination) varies depending on the location on earth and can be roughly obtained from the latest World Magnetic Model[5] of the earth’s magnetic field as a function of latitude and longitude. The industrial motion tracker accepts a setting of the declination value. This is done by setting the position in the MT Manager, SDK or by low-level communication. The yaw/heading will then be corrected for the declination calculated internally and thus referenced to “local” True North. The GNSS/INS products automatically set the current position when a GNSS-position fix is available. Therefore, the user does not have to insert it.

 

Velocity data

Velocity data, calculated by the sensor fusion algorithm, is provided in the same coordinate system as the orientation data (L<sub>XYZ</sub>), and thus adopts orientation resets as well (if any is applied). The velocity output is available in all GNSS/INS products (MTi-G-710, MTi-7, MTi-8, MTi-670(G), MTi-680(G), Xsens Avior GNSS/INS, Xsens Avior (Dual Antenna) RTK GNSS/INS, Xsens Sirius GNSS/INS, Xsens Sirius (Dual Antenna) RTK GNSS/INS, Xsens Avior Dual Antenna RTK GNSS/INS and Xsens Sirius Dual Antenna RTK GNSS/INS).

 

Note that the velocity data coming directly from the PVT (Position Velocity Time) data retrieved from any GNSS receiver provided with any Xsens development kit is represented in the NED reference frame. Different GNSS receivers may represent the velocity in different coordinate frames.

 

Position data

Position data, calculated by the sensor fusion algorithm, is represented in Latitude, Longitude and Altitude as in the WGS84 datum. The position output is available in all GNSS/INS products (MTi-G-710, MTi-7, MTi-8, MTi-670(G), MTi-680(G), Xsens Avior GNSS/INS, Xsens Avior RTK GNSS/INS, Xsens Sirius GNSS/INS, Xsens Sirius RTK GNSS/INS, Xsens Avior Dual Antenna RTK GNSS/INS and Xsens Sirius Dual Antenna RTK GNSS/INS).

 

It is possible to retrieve position data calculated by the sensor fusion algorithm in Earth Centered – Earth Fixed (ECEF) format. See figure Visualization of the local earth-fixed coordinate system and Position representation systems WGS84 for a visualization and the MT Low Level Communication Protocol Documentation for more information.

 

Calibrated ∆q and ∆v outputs

The calibrated ∆q (delta_q) and ∆v (delta_v) outputs are the coning and sculling compensated strapdown integrated data in the sensor-fixed coordinate system (Sxyz) or (Oxyz). Note that the value of the output depends on the output frequency, as the values are integrated over the sample time. These values represent the orientation change and velocity change during a certain interval based on the output rate. The output rate is selectable up to 100 Hz or 400 Hz depending on the product. Delta_q can also be noted as dq, delta_angle, del_q or OriInc. Delta_v can also be noted as dv, delta_velocity, del_v or VelInc.

 

Output specifications ∆q and ∆v outputs

Output

Unit

Delta_q (DataID 0x8030)

a.u. (quaternion values)

Delta_v (DataID 0x4010)

m/s

 

It is possible to multiply consecutive delta_q values to find the total orientation change over a specific period. Note that this data is not drift free, it still contains the sensor bias, as it has not been processed by the sensor fusion algorithm. Use the orientation output for drift free orientation.

 

Calibrated inertial and magnetic data outputs

Output of calibrated 3D linear acceleration, 3D rate of turn and 3D magnetic field data is in the sensor-fixed coordinate system (Sxyz) or (Oxyz). The units of the calibrated data output are as shown in the table Output specifications inertial and magnetometer data outputs.

 

Output specifications inertial and magnetometer data outputs

Vector

Unit

Acceleration (DataID 0x4020)

m/s2

Angular velocity (RateOfTurn) (DataID 0x8020)

rad/s

Magnetic field (DataID 0xC020)

a.u. (arbitrary units; normalized to earth field strength at the location the MFM is performed)

 

High-rate (HR) inertial data outputs

High-rate calibrated 3D acceleration (accelerometer) and 3D rate of turn (gyroscope) are outputted in the sensor-fixed coordinate system (Sxyz) or (Oxyz). The units of the calibrated data output are as shown in the table Output specifications high rate calibrated inertial data outputs. HR calibrated data is available at a higher rate than regular calibrated inertial data outputs. It is outputted as a separate data packet next to the other data outputs. The maximum output rate, degree of signal processing, and calibration applied depends on the device type.

Refer to MT Low Level Communication Protocol Documentation for more details.

 

Output specifications high rate calibrated inertial data outputs

Vector

Unit

AccelerationHR (DataID 0x4040)

m/s2

RateOfTurnHR (DataID 0x8040)

rad/s

 

 

Free acceleration

Free acceleration (Data ID 0x4030) is the acceleration in the local frame (LXYZ) from which the local gravity is deducted. The output is in m/s2.

 

Heave

Heave is the vertical displacement of the industrial motion tracker along the local-earth-fixed Z-axis (LXYZ), induced by wave motion acting on a vessel or platform. The heave output is zero-referenced (zero mean), meaning it represents relative vertical motion about the mean sea level rather than absolute altitude. The output is provided in real time at 100 Hz, converges within approximately 40 seconds of start-up, and achieves an accuracy of ≤ 5 cm for wave periods up to 29 seconds. Heave is available on the Xsens Sirius series and Xsens Avior series. Units can be found in the table output specifications heave. 

Output specifications heave

Vector

Unit

HeavePosition (DataID 0x6010)

cm

HeavePeriod (DataID 0x6020)

s

 

Xsens Sensor Fusion Algorithms

The orientation and position output of the VRU/AHT, AHRS and GNSS/INS are computed by Xsens’ proprietary sensor fusion algorithm. It uses signals from the rate gyroscopes, accelerometers, magnetometers and optionally a GNSS receiver and barometer to compute a statistical optimal 3D orientation and position estimates of high accuracy without drift for both static and dynamic movements.

 

The design of a typical algorithm can be summarized as a sensor fusion algorithm where the measurement of gravity (by the 3D accelerometers) and Earth's magnetic north (by the 3D magnetometers) compensate for otherwise slowly, but unlimited, increasing (drift) errors from the integration of rate of turn data (angular velocity from the rate gyroscope). This type of drift compensation is often called attitude and heading referencing and such a system is referred to as an Attitude and Heading Reference System (AHRS).

 

In products where a GNSS receiver is available, GNSS data is continuously used to aid the estimation of the device’s roll, pitch and heading next to position and velocity. An additional benefit is that short term GNSS outages can be coped with, through dead-reckoning, ensuring continuous data output. Such a system is referred to as GNSS/INS.

 

Internal Sensor Bias Estimation

The Xsens algorithm continuously estimates the gyroscope bias. For the rate of turn around the x-axis and the y-axis (roll and pitch axes), the gyroscope bias is estimated using gravity (accelerometers). In a homogenous magnetic field and with filter profiles using the magnetometer, the gyroscope bias around the z-axis will also successfully be estimated.

 

In some situations, the heading cannot be referenced to the Earth's magnetic field. This is the case when the magnetic field is not used (for example for VRU/AHT devices) or when the magnetic field is distorted. There are several ways to mitigate the drift in yaw (rotation around the z-axis):

  1. When the industrial motion tracker has sufficient movement in roll and pitch (>30 degrees for more than 10 seconds), the gyroscope bias will be estimated for the z-gyroscope. When rotating the device back to roll and pitch around 0 degrees, the yaw will be more stable than before the roll/pitch movements.
  2. The yaw drift can also be stabilized by using Active Heading Stabilization (AHS). Refer to section Additional setting options and features of this document for more details.
  3. It is also possible to estimate the gyroscope bias using the manual gyro bias estimation feature when the device does not rotate (also called No Rotation Update). More information about the Manual Gyro Bias Estimation feature can be found on BASE. For the MTi-680(G), an automated (non-user-initiated) version is available: the Continuous Zero Rotation Update (CZRU).

 

Roll and Pitch estimation

The Xsens sensor fusion algorithm stabilizes the inclination (i.e. roll and pitch combined) using the accelerometer signals. An accelerometer measures the specific force that is composed of the gravitational acceleration plus the linear acceleration due to the movement of the object with respect to its surroundings. The algorithm uses the assumption that on average the acceleration due to the movement is zero. Using this assumption, the direction of the gravity can be observed and used to stabilize the attitude. The orientation of the industrial motion tracker in the gravity field is accounted for such that centripetal accelerations or asymmetrical movements cannot cause a degraded orientation estimate performance. The key here is the amount of time over which the acceleration must be averaged for the assumption to hold. During this time, the gyroscopes must be able to track the orientation to a high degree of accuracy. In practice, this limits the amount of time over which the assumption holds true.

 

However, for some applications, this assumption does not hold. For example, an accelerating automobile may generate significant permanent accelerations for time periods lasting longer than the maximum duration the sensor’s rate gyroscopes can reliably keep track of the orientation. This may degrade the accuracy of the orientation estimates because the application does not match the assumptions made in the algorithm. Note, however, that as soon as the movement again matches the assumptions made, the algorithm will recover and stabilize. The recovery to optimal accuracy can take some time.

 

NOTE: To be able to accurately measure orientations as well as position in applications which can encounter long-term accelerations, we offer solutions that use aiding data from a GNSS receiver: the GNSS/INS products.

 

Heading/yaw estimation

By default, yaw is referenced by using the local (earth) magnetic field (e.g. in the AHRS product versions). In other words, the measured magnetic field is used as a compass. If the local Earth magnetic field is temporarily disturbed, the algorithm will track this disturbance instead of incorrectly assuming there is no disturbance. However, in the case of structural magnetic disturbance (>10 to 30 seconds, depending on the filter profile settings) the computed heading will slowly converge to a solution using the 'new' local magnetic north. Note that the magnetic field has no direct effect on the inclination estimate.

 

The filter profile ‘Fixed Mag Ref’ will assume a magnetic reference upon startup and keep that reference regardless of new magnetic environments (available on MTi 600-series, Xsens Avior series and Xsens Sirius series, see MTi 600-series Datasheet, Xsens Avior series Datasheet and Xsens Sirius series Datasheet).

 

In the special case the industrial motion tracker is rigidly strapped to an object containing ferromagnetic materials, structural magnetic disturbances will be present. In that case, Xsens offers an easy-to-use solution to recalibrate the magnetometers based on those structural magnetic disturbances (refer to chapter Magnetic materials and magnets of this document).

 

Next to the solutions described in the article Estimating Yaw in magnetically disturbed environments to mitigate effects of magnetic disturbances, the sensor fusion algorithm in a GNSS/INS device makes use of data from the GNSS receiver. This means that the GNSS/INS device has an increased resistance towards magnetic disturbances. It is for example possible to estimate the heading based on comparison between accelerometer data and the GNSS acceleration. For the MTi-7/8 and MTi-670(G)/680(G), the magnetometer data is only actively used in the GeneralMag filter profile; the other filter profiles are completely independent of the magnetic field. The Xsens Avior and Xsens Sirius GNSS/INS products use a filter profile combined with a selectable heading behaviour (NoMag or MagAided) that determines whether the magnetic field is used; refer to the respective datasheets.

 

The Xsens Avior Dual Antenna RTK GNSS/INS and Xsens Sirius Dual Antenna RTK GNSS/INS products compute heading directly from the baseline between two GNSS antennas. This heading is referenced to True North, independent of the magnetic field, and available at standstill and at low dynamics, as it does not require vehicle motion. Correct heading requires configuring the antenna baseline and lever arms. When GNSS heading is temporarily unavailable (e.g. due to signal blockage), the sensor fusion algorithm continues using the inertial data and the other available aiding sources.

 

Velocity and Position estimation

Transient accelerations

The GNSS/INS algorithm adds robustness to its orientation and position estimates by combining measurements and estimates from the inertial sensors and GNSS receiver in order to compensate for transient accelerations. It results in improved estimates of roll, pitch, yaw, position and velocity.

 
Loss of GNSS

When the GNSS/INS device has limited/mediocre GNSS reception or even no GNSS reception at all, the sensor fusion algorithm seamlessly adjusts the filter settings in such a way that the highest possible accuracy is maintained. The GNSS/INS industrial motion tracker will continue to output position, velocity and orientation estimates, although the accuracy is likely to degrade over time as the filters will have to rely on dead-reckoning. The GNSS status will be monitored continuously such that the filter can take GNSS data into account again when available and sufficiently trustworthy. In case the loss of GNSS lasts longer than a specific period (depending on product type, e.g. 45 seconds), the device will enter a state in which it stops outputting position and velocity estimates, and no longer uses velocity estimates in its sensor fusion algorithms until GNSS reception is re-established.

 

Heave

For marine applications, the Xsens sensor fusion algorithm can additionally estimate heave. The estimate is derived from the vertical component of acceleration, which is isolated from the inertial data using the orientation estimate so that the varying projection of gravity and the horizontal accelerations are accounted for when the device is subject to roll and pitch. Integrating this vertical acceleration yields velocity and displacement, but on a real sensor signal this alone is not sufficient, as small biases and noise accumulate and cause the estimate to drift and to lag the true motion in time. To compensate, an adaptive filter continuously estimates the dominant wave period and applies phase and amplitude corrections, so that the reported displacement remains aligned with the true vertical motion across changing sea states. The heave output is provided in real time at 100 Hz. As with the other estimates, the output requires some time to stabilize after the device is put into measurement mode; the filter converges within approximately 40 seconds of start-up, after which it achieves an accuracy of ≤ 5 cm for wave periods up to 29 seconds. The heave output is zero-referenced (zero mean), meaning it represents relative vertical motion about the mean sea level rather than absolute altitude.

 

Initialization

The Xsens sensor fusion algorithms not only estimate orientation, but also keep track of variables such as sensor biases or properties of the local magnetic field. For this reason, the orientation output may need some time to stabilize once the industrial motion tracker is put into measurement mode. Time to obtain optimal stable output depends on a number of factors. An important factor determining stabilizing time is determined by the time to correct for small errors in the bias of the gyroscopes. The bias of the gyroscope may slowly change due to different effects such as temperature change or exposure to impact.

For the MTi-7/8/670(G)/680(G), it is highly recommended to set the initial heading (Yaw) of the device after power-up. Refer to the MTi-1-series/MTi 600-series Datasheet or the SetInitialHeading command in the MT Low-Level Communication Protocol Documentation for more information. For the Xsens Avior Dual Antenna RTK GNSS/INS and Xsens Sirius Dual Antenna RTK GNSS/INS, setting an initial heading is not required once a valid GNSS heading is available.

 

Filter Profile options

As described above, the algorithm uses assumptions about the acceleration and the magnetic field to obtain orientation. Because the characteristics of the acceleration or magnetic field differ for different applications, the Xsens algorithm makes use of filter profiles to be able to use the correct assumptions given the application. This way, it can be optimized for different types of movement. For optimal performance in a given application, the correct filter profile must be set by the user. Each product offers different filter profile options. Refer to the specific documentation to know more about the filter profiles[7].

 

Additional settings, options and features

The table below summarizes the additional options offered to adapt and optimize the algorithm to cover more scenarios and possible corner cases.

 

 

Supplementary features and settings

Active Heading Stabilization (AHS)

Active Heading Stabilization (AHS) is a software component within the sensor fusion engine designed to give a low-drift unreferenced (not North-referenced) yaw solution even in a disturbed magnetic environment. It is aimed to tackle magnetic distortions that do not move with the sensor, i.e. temporary or spatial distortions.

 

AHS is not tuned for nor intended to be used with GNSS/INS devices. Therefore, Xsens discourages the use of this feature for GNSS/INS devices.

 

For the MTi 600-series, Xsens Avior series and Xsens Sirius series, the AHS feature is embedded in the filter profiles.

 

For more information on the activation and use of AHS, refer to the BASE-article: BASE by Xsens - AHS tutorial

Orientation Smoother

 

The Orientation Smoother is a software component within the sensor fusion engine that is currently only available for the MTi-670(G), MTi-680(G), MTi-G-710, and the Xsens Avior (Dual Antenna) (RTK) GNSS/INS and Xsens Sirius (Dual Antenna) (RTK) GNSS/INS products. This feature aims to reduce any sudden jumps in the Orientation outputs that may arise when fusing low-rate GNSS receiver messages with high-rate inertial sensor data.

 

The Orientation Smoother can be enabled from the Device Settings window in MT Manager, or by using the setOptionFlags low-level command (see MT Low Level Communication Protocol Documentation).

 

Position / velocity Smoother

The Position/velocity Smoother is a software component within the sensor fusion engine that is currently only available for the MTi-680(G), the Xsens Avior (Dual Antenna) RTK GNSS/INS and the Xsens (Dual Antenna) Sirius RTK GNSS/INS. This feature aims to reduce any sudden jumps in the position outputs that may arise when fusing low-rate GNSS receiver messages with high-rate inertial sensor data.

 

The Position/velocitySmoother can be enabled from the Device Settings window in MT Manager, or by using the setOptionFlags low-level command (see MT Low Level Communication Protocol Documentation).

GNSS Platform

u-blox GNSS receivers support different dynamic platform models in order to adjust the navigation engine to the expected application environment. The GNSS/INS products can be configured to communicate a desired platform model upon start-up. This enables the user to adjust the u-blox receiver platform to match the dynamics of the application. The setting influences the estimates of Position and Velocity and, therefore, it affects the behavior of the Xsens filter output.

 

The platform model can be configured using MT Manager or low-level communication by providing the GNSS Platform ID. For more details on the low-level commands used to set the GNSS Platform (SetGnssPlatform for the MTi-7/8 and SetGnssReceiverSettings for the MTi-670/680(G) and the Xsens Avior and Xsens Sirius GNSS/INS products), refer to the MT Low Level Communication Protocol Document. For more details on GNSS platform settings, refer to the u-blox Receiver Description Manual.

 

Alternatively, on the MTi-670/680 and the Xsens Avior (Dual Antenna) (RTK) GNSS/INS products, when interfacing with a GNSS receiver through other communication protocols than UBX (u-blox), the position data is used 'as is', independent of the GNSS platform setting.

In-run Compass Calibration (ICC)

 

In-run Compass Calibration (ICC) provides a solution to calibrate the sensor for magnetic distortions caused by objects that move with the industrial motion tracker . Examples are the cases where the industrial motion tracker is attached to a car, aircraft, ship or other platforms that can distort the magnetic field. It also handles situations in which the sensor has become magnetized. ICC is an alternative to the offline MFM (Magnetic Field Mapper). It results in a solution that can run embedded on different industrial platforms (leaving out the need for a host processor like a PC) and relies less on specific user input.

ICC is currently a feature in beta. For more information, refer to the BASE-article on ICC: BASE by Xsens - ICC Tutorial.

 

Continuous Zero Rotation Update (CRZU)

The Continuous Zero Rotation Update (CZRU) is a feature that is currently only available for the MTi-680(G) and Xsens Sirius/Avior (Dual Antenna) (RTK) GNSS/INS. The purpose of the CZRU is to reduce the undesired effects of gyroscope bias, such as drift of the orientation output. Although all industrial motion tracker products are individually calibrated for various parameters, including sensor bias, the aging and use of Motion Trackers in industrial environments can cause sensor biases to change during the product's lifetime. Because of that, the filters of the industrial motion tracker are continuously re-estimating calibration parameters such as sensor bias while they are powered up. If enabled, the Continuous Zero Rotation Update will execute a background algorithm that will automatically initiate a gyroscope bias estimation sequence whenever the Motion Tracker is motionless. 

Note: For Xsens Sirius/Avior (RTK) GNSS/INS products the CZRU is embedded in the filter profiles.

 

The Continuous Zero Rotation Update can be enabled through the Device Settings window in MT Manager, or through the SetOptionFlags low-level command (see MT Low Level Communication Protocol Document).

 

 

 

Series interface options

The industrial motion tracker series product lines are able to communicate and output data via many different interfaces. The table below provides a convenient overview for the MTi 1-series, MTi 600-series, Xsens Avior series and Xsens Sirius series. Details on the interfaces for each product are available in the respective datasheets or hardware integration manuals.

 

 

 

Overview of interface options in MTi portfolio

Interface

MTi 1-series

MTi-320

MTi 600-series modules

MTi-630R, MTi-670G, MTi-680G

Avior

series

Sirius series

I²C

•

   

 

•  

SPI

•

   

 

•  

UART

•

 

•

 

•  

USB

Development Board

Via cable and USB converter

Development Board or UART2USB Converter

Via cable and USB converter

  Via cable

RS232

  •

•

•

• •

RS485

     

 

   

RS422

   

Dev. Board

 

Dev. Board •

CAN

   

•

•

• •

 

 

Please note: the RS232 and RS422 are available depending on the model, but a model with RS232 will not have RS422, and vice versa.

 

Timing and synchronization

The industrial motion tracker products support multiple features for synchronizing data with external devices and timing. Please refer to the respective datasheets or manuals for more information.

 


[1] Also known as “g-sensitivity”.

[2] The default reference coordinate system LXYZ only applies to the industrial motion tracker in Normal (Xbus) or CAN output mode. Refer to the Low Level Communication Protocol Documentation for detailed orientation output specifications when using the ASCII (NMEA) output mode.

[3] Please note that, due to the definition of Euler angles, there is a mathematical singularity (gimbal lock) when the sensor-fixed x-axis is pointing up or down in the earth-fixed reference frame (i.e. pitch approaches ±90°). In practice, this means roll and pitch is not defined as such when pitch is close to ±90 deg. This singularity is in no way present in the quaternion or rotation matrix output mode.

[4] IEEE Std 1559TM-2009: IEEE Standard for Inertial Systems Terminology

[5] Xsens releases a firmware update when a new WMM version is available

[6] The barometer and GNSS receiver do not require additional calibration.

[7] Datasheet for the MTi 1-series, MTi 600-series, Xsens Avior series and Xsens Sirius series. MTi User Manual for the other Xsens MTi products

 

 
Create your own Knowledge Base