This section describes the (mechanical) design and hardware integration considerations of the Xsens Sirius series devices. 3D models of the robust trackers are available and found on BASE.
The Xsens Sirius series uses a right-handed coordinate system as the basis of the sensor frame. The default sensor coordinate system is printed on the side of the device and is indicated in the figures below. More details regarding (the modification of) the reference frames of the device can be found in the Xsens Sirius series Datasheet and Family Reference Manual.

Default sensor coordinate system for the Xsens Sirius IMU/VRU/AHRS

Default sensor coordinate system for the Xsens Sirius (RTK) GNSS/INS

Default sensor coordinate system for the Xsens Sirius Dual Antenna RTK GNSS/INS
The accelerometer determines the origin of measurements. The
in the figures below shows the location of the accelerometer of the Xsens Sirius series module and robust trackers.

Location origin of measurements for Xsens Sirius IMU/VRU/AHRS

Location origin of measurements for Xsens Sirius (RTK) GNSS/INS

Location origin of measurements for Xsens Sirius Dual Antenna RTK GNSS/INS
The Xsens Sirius series only supports wire connectors. The devices only feature the 12-pin ODU connector for main supply and communication.
All robust trackers have three (M3) mounting holes to mount them on a flat surface. The figures below show the connector and mounting hole positions on the Xsens Sirius devices.
Xsens Sirius IMU/VRU/AHRS connector and mounting hole positions (dimensions in mm)
The figures below show examples of the Xsens Sirius IMU/VRU/AHRS mounted on a surface.

Xsens Sirius IMU/VRU/AHRS mounting example (dimensions in mm)
The figure below shows an example of the Sirius GNSS mounted on a surface. The M3 screws should not be tightened with more than 1 Nm. It is recommended to use a thread locking material (especially in high vibration environments).

Xsens Sirius (RTK) GNSS/INS mounting example (dimensions in mm)
|
Part |
Manufacturer |
Part number |
Description |
|---|---|---|---|
|
Host Interface connector |
ODU |
A10WAM-P12XMM0-0000 |
AMC HD, break-away, 12 circuits |
|
ODU |
C10WAM-P12XMM0-0000 |
AMC HD, screw lock, 12 circuits |
|
|
Screws |
|
|
Brass, M3 x 6 mm |
The following cables can be ordered from Xsens.
CA-MP-USB (For Sirius IMU/VRU/AHRS)
The CA-MP-USB cable is a RS232 to USB cable that has the USB converter integrated at the end of the cable and consists of the following parts:
The table below shows the pinning of the connections.
|
Function |
Wire colour |
ODU pin no. |
|
VIN |
Red |
5 |
|
GND |
Black |
10 |
|
RS232_ RTS |
Violet |
9 |
|
RS232_ TxD |
Yellow |
8 |
|
RS232_RxD |
Grey |
7 |
|
RS232_CTS |
Orange |
6 |
|
SYNC_IN2 |
Red/White |
4 |
|
GND |
Blue |
12 |
|
SHIELD |
- |
SH |
The figures below show the cable length definition (from connector end-to-end).
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvMjAyNS9pbWFnZSgxOCkucG5nIiwiQ29uZGl0aW9uIjp7IkRhdGVMZXNzVGhhbiI6eyJBV1M6RXBvY2hUaW1lIjoxNzkzMjc0NzM4fX19XX0_&Signature=mz4OBzQATH4PCLhHypBJhDVVTBN7KeQ59R9MsqfJZMOvHnCIvV8sHneEhJRqT2TNskBuwxA3UqfDrBJ0H-JZkXaYjCpkYonN5CJYFRa7mmR1C5fqV2-XpFuQFEvJeTXUdiEV0iYmxrW25eXNSWR6pkOtl1K2uqtRrOlTmtKZsv7jcZcD6bBTrqx-tMKFA6vprFjXuzWJJ8O2yM2swW6ivJDIgyFrcxJ6Cvpy~m-KfpWMyegj31F9T1w1-mEzg-uIi1LMx2sjD1rOh4Di5lG2TbEWnlWS55sNQaC8AhREpOMFEroVEU3cvnCUtv-8Qli2jQeH6HBpjaV9DCVcXffIJg__&Key-Pair-Id=K2TK3EG287XSFC)
Host Interface cable CA-MP-USB length definition
CA-MP-USB-V2 (For Sirius (RTK) GNSS-INS)
The CA-MP-USB cable is a RS232 to USB cable that has the USB converter integrated at the end of the cable and consists of the following parts:
The table below shows the pinning of the connections.
|
Function |
Wire colour |
ODU pin no. |
|
VIN |
Red |
5 |
|
GND |
Black |
10 |
|
RS232_ RTS |
Violet |
9 |
|
RS232_ TxD |
Yellow |
8 |
|
RS232_RxD |
Grey |
7 |
|
RS232_CTS |
Orange |
6 |
|
PPS_OUT |
Red/White |
4 |
|
GND |
Blue |
12 |
|
SHIELD |
- |
SH |
The figures below show the cable length definition (from connector end-to-end).
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvMjAyNS9pbWFnZSgxOCkucG5nIiwiQ29uZGl0aW9uIjp7IkRhdGVMZXNzVGhhbiI6eyJBV1M6RXBvY2hUaW1lIjoxNzkzMjc0NzM4fX19XX0_&Signature=mz4OBzQATH4PCLhHypBJhDVVTBN7KeQ59R9MsqfJZMOvHnCIvV8sHneEhJRqT2TNskBuwxA3UqfDrBJ0H-JZkXaYjCpkYonN5CJYFRa7mmR1C5fqV2-XpFuQFEvJeTXUdiEV0iYmxrW25eXNSWR6pkOtl1K2uqtRrOlTmtKZsv7jcZcD6bBTrqx-tMKFA6vprFjXuzWJJ8O2yM2swW6ivJDIgyFrcxJ6Cvpy~m-KfpWMyegj31F9T1w1-mEzg-uIi1LMx2sjD1rOh4Di5lG2TbEWnlWS55sNQaC8AhREpOMFEroVEU3cvnCUtv-8Qli2jQeH6HBpjaV9DCVcXffIJg__&Key-Pair-Id=K2TK3EG287XSFC)
Host Interface cable CA-MP-USB-V2 length definition
CA-MP-USB-422
The CA-MP-USB-422 cable is a RS422 to USB cable that has the USB converter integrated at the end of the cable and consists of the following parts:
The table below shows the pinning of the connections.
|
Function |
Wire colour |
ODU pin no. |
|
VIN |
Red |
5 |
|
GND |
Black |
10 |
|
RS422_TX(+) |
Violet |
9 |
|
RS422_TX(-) |
Yellow |
8 |
|
RS422_RX(+) |
Grey |
7 |
|
RS422_RX(-) |
Orange |
6 |
|
SYNC_IN2 |
Red/White |
4 |
|
GND |
Blue |
12 |
|
SHIELD |
- |
SH |
The figures below show the cable length definition (from connector end-to-end).
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvMjAyNS9pbWFnZSgxNykucG5nIiwiQ29uZGl0aW9uIjp7IkRhdGVMZXNzVGhhbiI6eyJBV1M6RXBvY2hUaW1lIjoxNzkzMjc0NzM4fX19XX0_&Signature=eSDijMCFAme~3pheWNYfJGF9fWGcLGnce0nYTgd2RulBvcOlE2IRZPv51kmyq-RXAWpXXALuwjPPQfT~W9duFaPqLqViny1Fm0LQk27-triIKtJHks74qjiYJ0B7hIX3uMQ9Y4n2YqQSsGgfqBa50dwA0QYOJqw2zxuEQCK~cu~v5m0MDwbYPFQn3L5iEsmidEEsB3lAD-~IVnbgdD2m60feW2D8GveNb1sNl54gCGdCXyJSTmG7SS-2KhGqMoLAHdh4f~LJxVcLLi8G-mQhYdGV-UXjiGVWE2LsoG6E7VnU~ySUp8YzgKrTf9kiBB0iAnKhm7hbq0DZWvJxxweMfg__&Key-Pair-Id=K2TK3EG287XSFC)
Host Interface cable CA-MP-USB-422 length definition
CA-MP-12-OPEN
The CA-MP-12-OPEN is a 12-pin Host Interface pigtail cable that consists of the following parts:
The table below shows the pinning of the connections. The shield of the cable is only connected on the ODU connector side.
|
Function |
Wire colour |
ODU pin no. |
|
VIN |
Red |
5 |
|
GND |
Black |
10 |
|
CAN_H |
Green |
1 |
|
CAN_L |
White |
2 |
|
RS232_RTS/RS422_TX(+) |
Violet |
9 |
|
RS232_TxD/RS422_TX(-) |
Yellow |
8 |
|
RS232_RxD/RS422_RX(+) |
Grey |
7 |
|
RS232_CTS/RS422_RX(-) |
Orange |
6 |
|
SYNC_IN1 |
Black/White |
3 |
|
SYNC_IN2 |
Red/White |
4 |
|
SYNC_OUT |
Blue/White |
11 |
|
GND |
Blue |
12 |
|
SHIELD |
- |
SH |
The figures below show the cable length definition (from connector end-to-end) and the pinning of the ODU connector.

Host Interface cable length definition
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvaW1hZ2UoMTMyKS5wbmciLCJDb25kaXRpb24iOnsiRGF0ZUxlc3NUaGFuIjp7IkFXUzpFcG9jaFRpbWUiOjE3OTMyNzQ3Mzh9fX1dfQ__&Signature=Sw~kWvWUpkMqaAgifxD-filUaHZN0xZPyMlyGaDhMKWqTpQeJWR-XjRic44jV3Avktt5tfkIknGyovCYknTku6OCtn9uUQ~oEsjRGrcquzAwLqAS9Tp~EBHRdU-ZZL~dObFfcIT09OmpHsGpVzXhhhU1L7SA4bcHVb4uYsM-Bntp6zvvP5rtyawPlpL-RbxIUG2KJdVtFaXjKUU0SD5noMD0Q0M4zD2dkGUYm6rHxDmniSIX1Cpm9nC15CvGBmJH9xKpHozwioxhbQH4wCNWH~i4rt5ygmZNBuaT1kGs4OwbcWRa~4E2ySNVaAkU60DUcP9ju1yHQZd0ZQzKkHsONg__&Key-Pair-Id=K2TK3EG287XSFC)
Numbering 12-pin ODU connector (solder cup view).
CA-MP-MTI-4
The CA-MP-MTI-4 is the RTCM corrections cable that consists of the following parts:
Molex connector: 2045320401; 1.25mm pitch, single row, positive lock, 4 circuits
ODU connector: A1CWAM-P04XBC0-0000; AMC HD, break-away plug, 4 circuits
Cable: 2.9 m, 12 core, AWG28, shielded, UL, -40ºC - +85ºC
Molex crimp terminals: 5054311100; gold (Au) plating, 26-30 AWG
The table below shows the pinning of the connections. The shield of the cable is only connected on the ODU connector side.
|
Function |
Wire colour |
Molex pin no. |
ODU pin no. |
|
V_BCKP |
Red |
1 |
1 |
|
GND |
Black |
2 |
2 |
|
RTCM_TxD |
Green |
3 |
4 |
|
RTCM_RxD |
White |
4 |
3 |
|
SHIELD |
- |
- |
SH |


The Xsens Sirius series samples IMU signals at 10kHz per channel, processing them using a strapdown integration algorithm with coning/sculling compensation. Proper coning/sculling compensation already mitigates errors that poorly designed signal processing pipelines introduce when the device is under vibration. For best results, however, it is recommended that the Sirius products be mechanically isolated from vibrations as much as possible: since vibrations are measured directly by the accelerometers, the following two conditions can make the readings from the accelerometers invalid;
There is an effect on the gyroscopes as well and, especially when the vibrations include high-frequent coning motion, the gyroscope readings may become invalid. The Xsens Sirius series features mechanical vibration rejecting gyroscopes, designed to better cope with these specific conditions.
Xsens has tested a set of vibration dampeners. Vibration dampeners are low-profile rubber cylinders that allow the Xsens Sirius series to be mounted on an object without a direct metal to metal connection that transduces vibrations from the object to the Xsens Sirius series. The vibration dampeners have been tested with frequencies up to 1200 Hz that caused aliasing when the Xsens Sirius series was mounted directly on the vibration table. These vibrations had no effect with the vibration dampeners fitted. The dampeners tested are manufactured by Norelem and have part number 26102-00800855, www.norelem.com
When the Xsens Sirius motion tracker is placed close to or on an object that is either magnetic or contains ferromagnetic materials, the measured magnetic field is distorted (warped) and causes an error in the computed yaw. The earth's magnetic field is altered by the presence of ferromagnetic materials, permanent magnets or power lines with strong currents (several amperes) in the vicinity of the device. The distance to the object and the amount of ferromagnetic material determines the magnitude of disturbance introduced. Errors in estimated yaw due to such distortions can be quite large, since the earth's magnetic field is very weak in comparison to the magnitude of the sources of distortion.
For more information on how to mitigate the detrimental effects of magnetic distortion, refer to the BASE article Estimating Yaw in magnetically disturbed environments.