The Vision Navigator has three LEDs to indicate the current status of the sensor.

Ethernet connector standard

I/O connector pin overview
|
Pin |
Wire color |
Symbol |
Description |
|---|---|---|---|
|
1 |
Red |
CANH |
CAN High #1 |
|
2 |
White |
CANL |
CAN Low |
|
3 |
Green |
PWR_SHDN |
Power shutdown #2 |
|
4 |
Black or Grey |
GND |
Signal ground |
|
5 |
Blue |
TM_PLS |
GNSS1 receiver time pulse |
|
6 |
Yellow |
TM_MRK |
Power shutdown #3 |
|
7 |
Orange or Pink |
UART1_RX |
UART receiver input 1 |
|
8 |
Brown |
UART1_TX |
UART transmitter output 1 |
The UART1 interface on the I/O connector is configured to 3.3 V logic levels. The user must ensure that the connected device also uses 3.3 V logic levels to avoid damage to the XVN. It is possible to convert the logic levels to support RS-232 using adequate equipment. Please see the web documentation from Fixposition here.

AUX connector pin overview
|
Pin |
Wire color |
Symbol |
Description |
|---|---|---|---|
|
1 |
Red |
+5V |
Voltage supply output of 5V |
|
2 |
White |
UART2_RX |
UART receiver input 2 |
|
3 |
Green |
UART2_TX |
UART transmitter output 2 |
|
4 |
Black or Grey |
GND |
Signal ground |
|
5 |
Blue |
Reserved |
Reserved |
|
6 |
Yellow |
Reserved |
Reserved |
|
7 |
Orange or Pink |
Reserved |
Reserved |
|
8 |
Brown |
Reserved |
Reserved |
The UART2 interface on the AUX connector is configured to 3.3 V logic levels. The user must ensure that the connected device also uses 3.3 V logic levels to avoid damage to the XVN. It is possible to convert the logic levels to support RS-232 using adequate equipment. Please see the web documentation from Fixposition here.

|
Pin |
Wire color |
Symbol |
Description |
|---|---|---|---|
|
1/2 |
Black |
GND |
Power ground |
|
3/4 |
Red |
VCC |
Main power input |
The Vision Navigator contains two GNSS receivers that can connect to an antenna via the female SMA connectors labeled GNSS 1 and GNSS 2.
The Vision Navigator can significantly increase its Wi-Fi range by connecting a Wi-Fi antenna to the female RP-SMA connector labeled Wi-Fi.
The Vision Navigator contains a USB-C port to connect an external drive for data recording. With firmware version 2.63 and later, the user can also use this port to access the recovery mode (see Sensor configuration).Note that the USB-C port must only be used as a service interface, not during operation.