The user can select which messages are assigned to each port at the "Output messages" module inside the "Configuration → I/O" panel, as shown in the following image:
.png?Policy=eyJTdGF0ZW1lbnQiOlt7IlJlc291cmNlIjoiaHR0cHM6Ly9kemY4dnF2MjRlcWhnLmNsb3VkZnJvbnQubmV0L3VzZXJmaWxlcy8yNzc1NC8zNTEzNS9ja2ZpbmRlci9pbWFnZXMvcXUvaW1hZ2UoNTc5KS5wbmciLCJDb25kaXRpb24iOnsiRGF0ZUxlc3NUaGFuIjp7IkFXUzpFcG9jaFRpbWUiOjE3ODQ2ODQ3OTF9fX1dfQ__&Signature=kLGfprwiGLYTLBC3zU4aN3xJNY3~V-6obdktjiIyCYMtCX3SRviQ~75PID~G5kjD2lOhtbJu7rn84ZZ~cE80Q8nrL-p-WzQ0rX8le-X5IY4MBuaEsQeou29OZCYyTpE3E64JZnwfPqrRU1HbaXZsHjbdKXygiKnULNOeTJLEPwpZyy34Ir1uE73dvn50AmZJQXQh-g6AGNiV2720BqdTHz6arxfAzBOJtT34K05O~ZQP79xhtn-rcbSZ0EL41mXANPpkMW9GpG-3TvlU3moTJTvEKJqA4jW94hElWAL0VZ4uO9Wbgyan3qP-QEXMXbRU86sFuD3hjX5WtJRVNCzImQ__&Key-Pair-Id=K2TK3EG287XSFC)
Output message configuration on the web interface
The output frequency of these messages is the same as the Fusion output frequency configured in the output generator (See Input/output system overview for more information). By default, the output frequency is 10 Hz, but the user can configure it to the range of 1-100 Hz.
Available Fusion messages:
All IMU output is generated at the IMU frequency of approximately 200 Hz. Note that the IMU output requires a lot of output bandwidth. For example, on a serial port, the baud rate must be set high enough for the necessary bandwidth. The exact number depends on what messages are enabled for the port.
Available IMU messages:
The output frequency of these messages is 1 Hz. See exceptions below.
Available TF messages:
∗ The output frequency of this message is the same as the configured Fusion frequency, see Output generator.
∗∗ The output frequency of this message is 200Hz.
Text output is an irregular output of text messages (strings). There are four levels:
ERROR – Errors. An error is something from which the sensor cannot recover or something that renders the sensor unusable in normal circumstances.
WARNING – Warnings. A warning is something from which the sensor could recover or something that does not render the sensor unusable in normal circumstances (i.e., the sensor operated to specifications). But it can, for example, hint at degraded performance.
INFO – General information.
DEBUG – Debug information valuable to the support team.
For example, the sensor outputs a "boot screen" on boot. While it does output it to any port where the FP_A-TEXT_INFO message is enabled, it is only practical to observe this output on UART and CANSTR ports. It is not possible to connect to the TCP ports in time to observe this output.
The boot screen is as follows:
$FP,TEXT,1,INFO,Fixposition AG - www.fixposition.com*09rn
$FP,TEXT,1,INFO,SW=fp_release_vr2_2.61.0_191*78rn
$FP,TEXT,1,INFO,HW=nav-vr2 1.2a 6d9d18*3Ern
Available text messages:
All GNSS output is generated by default at the GNSS frequency of approximately 5 Hz. In addition, some GNSS output messages cannot be distinguished between GNSS receivers; ensure you use different ports to avoid confusion.
Available GNSS messages: